Boost your projects with new IoT RedBoards and Python support!
View in browser
SparkFun Logo
WHAT'S NEW    TOP SELLERS    QWIIC    MICROMOD    REDBOARDS    THING+    TUTORIALS
27708-Redboard-RP2350-Feature

The SparkFun RP2350 IoT Redboard combines the Raspberry Pi® RP2350 microcontroller with the Raspberry Pi® RM2 radio module to provide a powerful and versatile wireless development platform in the Arduino R4 form factor. This IoT RedBoard also includes integrated battery power and charging circuits, µSD card slot, Qwiic connector, 3-pin debug header, as well as a 22-pin ribbon cable connector tied to the RP2350's HSTX (high-speed transmit) pins. The board shares a pinout between female headers and matching 0.1"-spaced plated through-hole (PTH) headers to allow you to choose between temporary or soldered connections.

Wireless IoT? Plentiful PSRAM? Get the RP2350 IoT Redboard now!

28434-Redboard-Iot-ESP32-Micropython-Feature

This SparkFun ESP32 IoT RedBoard version is an ESP32 Development Board specially programmed to run MicroPython out of the box. It makes it easy to get started using SparkFun's 40+ MicroPython-capable modules. The ESP32-D0WDQ6 chip, designed to be both scalable and adaptive, is at the core of this module. The IoT RedBoard can target various applications, ranging from low-power sensor networks to the most demanding tasks, such as voice encoding, music streaming, and MP3 decoding. The IoT ReadBoard also utilizes our handy Qwiic Connect System, which means no soldering or shields are required to connect it to the rest of your system!

For a limited time, when you purchase the SparkFun IoT RedBoard—ESP32 MicroPython Development Board—you receive a free Precision Temperature Sensor & 50mm Qwiic Cable!

Add all three items to your cart, and the TMP117 and Qwiic Cable will be free at check-out.

Customer accounts only. Promotion valid while suppliers last.

15805-SparkFun_High_Precision_Temperature_Sensor_-_TMP117__Qwiic_-01-1
14426-Qwiic_Cable_-_50mm-01
ESP32 IoT RedBoard: Now Standard with MicroPython!

unnamed-Mar-20-2025-06-03-58-8189-PM

Exciting news for embedded developers! SparkFun is thrilled to announce a significant expansion of our software support with the launch of 47 new Python libraries that support both Python and MicroPython. This comprehensive collection empowers users to seamlessly integrate Python and MicroPython into their projects across a wide range of popular platforms. From sensor interfacing to intricate control systems, these libraries streamline development and bring the power of Python’s simplicity and versatility to SparkFun’s extensive sensor ecosystem. Whether you’re on the latest Raspberry Pi 5 or one of our latest MicroPython-enabled development boards, these new Python drivers from SparkFun open the world of rapid and dynamic prototyping using our latest sensor products.

SparkFun <3 Python & MicroPython

28020-RFID-USB-C-Reader-feature

The SparkFun RFID USB-C Reader provides a streamlined solution for reading low-frequency RFID tags. This user-friendly breakout board, featuring a USB-C connector and a reliable CH340C USB-to-serial chip, is designed for seamless integration with ID-Innovations Tiny RFID modules (excluding Mifare and ID-3XX models marked with an “MF”). It includes integrated LED and buzzer indicators for clear read confirmations, which can be easily disabled to suit your preferences. This Reader also supports multiple output formats, including the default ASCII, Magnetic Emulation, and Wiegand26, offering greater flexibility for diverse applications.

It's never been easier to connect to RFID!

27842-Beginner-Parts-Kit-Box-Feature

The SparkFun Beginner Parts Kit is a small container of parts frequently used by beginning (or even experienced) hobbyists that gives you all of the essential through-hole components you will need to get started playing with embedded projects. These are the "bubble gum" parts we regularly use or have often seen requested in class. Inside this kit, you will find a good starter assortment of caps, ICs, regulators, diodes, and good-for-blinky LEDs. This kit also features our Adjustable Parts Box for better organization.

An updated and refresher Beginner's Parts Kit

690-DOTW2025-Newsletter

Deal valid until March 27, 2025 @ 11:59 p.m. MDT

Product_XRP_play

Have you had a chance to explore the potential of the Experiential Robotics Platform (XRP)? If not, now is the perfect time! We recently released a video introducing you to the power and versatility of this comprehensive robotics platform, and we want to make sure you don't miss out.

A Closer Look at XRP
YouTube
Instagram
Twitter
facebook
LinkedIn
github-logo

SparkFun Electronics, 6333 Drycreek Pkwy, Niwot, CO 80503, (303) 284-0979

Unsubscribe Manage preferences