SX1276
The SX1276/77/78/79 transceivers feature the LoRa® long range modem that provides ultra-long range spread spectrum communication and high interference immunity whilst minimizing current consumption.
Using Semtech’s patented LoRa modulation technique SX1276/77/78/79 can achieve a sensitivity of over -148dBm using a low cost crystal and bill of materials. The high sensitivity combined with the integrated +20dBm power amplifier yields industry leading link budget making it optimal for any application requiring range or robustness. LoRa also provides significant advantages in both blocking and selectivity over conventional modulation techniques, solving the traditional design compromise between range, interference immunity and energy consumption.
Features
- LoRa Modem
- 168dB maximum link budget
- +20dBm - 100mW constant RF output vs. V supply
- +14dBm high efficiency PA
- Programmable bit rate up to 300kbps
- High sensitivity: down to -148dBm
- Bullet-proof front end: IIP3 = -11dBm
- Excellent blocking immunity
- Low RX current of 9.9mA, 200nA register retention
- Fully integrated synthesizer with a resolution of 61Hz
- FSK, GFSK, MSK, GMSK, LoRa and OOK modulation
- Built-in bit synchronizer for clock recovery
- Preamble detection
- 127dB Dynamic Range RSSI
- Automatic RF Sense and CAD with ultra-fast AFC
- Packet engine up to 256 bytes with CRC
- Built-in temperature sensor and low battery indicator
- Automated Meter Reading
- Home and Building Automation
- Wireless Alarm and Security Systems
- Industrial Monitoring and Control
- Long range Irrigation Systems
Applications
Packaging
- QFN 28
Order Codes
- SX1276IMLTRT - Pb-free, Halogen free, RoHS/WEEE compliant product
Pb(Lead)-Free/RoHS-Green Info
(-40°C to +85°C / 4000 cycles)
(50°C, 4000 Hrs)
Related Parts
SX1276IMLTRT
Datasheets & Documentation
Application Notes
Distributor/Catalog Supplier Inventory
View product availability from participating distributors below. Browse all distributers here.
Part # | Country | Qty | Buy | Distributor |
---|
Resources
To see more videos Videos
LoRaWAN® Relay: A Low-Cost, Battery-Powered Network Extender
READ NOWWhy LoRaWAN® Is Key to AMI Network Systems
READ NOWWater Sanitation For All With LoRa
READ NOWEnsuring Reliable Gas Supply and Increasing Infrastructure Safety
READ NOWOptimize Building Management
READ NOWCold Chain Monitoring
READ NOWThe LoRaWAN-based gateway is the physical layer (PHY) interface for the LoRaWAN network server (LNS). On the one hand, it listens to certain parts of the radio spectrum and decodes LoRa®-modulated signals originating from LoRa-based sensors. On the other hand, the gateway transmits messages from the network down to a sensor as LoRa-modulated signals.
The exact parameters which govern the reception and transmission of these signals is specified in the LoRaWAN Regional Parameters. The parameters are regionally differentiated because there are different regulatory requirements in different regions of the world.
Expert Series: 5 Things You Need to Know about…
READ NOWThe recently announced LoRa Basics™ Modem v4 feature release includes a powerful new feature – relay. It allows customers to add battery-operated, easy-to-deploy relay nodes that act as network extenders. These relay nodes can be placed in remote locations or in areas where signal strength is weak due to extreme distances or circumstances, effectively extending the range of existing gateway(s) and networks using LoRaWAN® connectivity.
READ NOWTo begin working with LoRa technology on Amazon Sidewalk, Amazon Sidewalk developers will need specific development kits, such as those provided by Silicon Labs, and Nordic Semiconductor. Both companies offer comprehensive Sidewalk development kits that can help you get started with LoRa and Amazon Sidewalk right away.
Amazon Sidewalk Prerequisites and Development Kits
READ NOWIntensive pig farming, also known as the ‘intensive piggery system’, has become the primary method of farming in the pig industry. According to this method, pigs are housed indoors and confined in individual stalls or straw-lined sheds at high stocking density, while keeping pigs of similar ages to live together in large crowds under common environmental settings. By doing so, feeding efficiency is significantly improved, and emerging technologies are often employed to maintain pig health and safeguard pig growth - monitoring various environmental parameters inside the barns with wireless temperature and humidity sensors is an exemplary case in point.
Stal Data Monitors Environmental Conditions and…
READ NOWAccording to the Ministry of Industry and Information Technology of the People's Republic of China, China's 5G network coverage continues to expand. Large-scale deployment of the 5G network strengthens the Internet of Things (IoT) ecosystem, extending IoT application scenarios to diversified fields including manufacturing, agriculture, medical care, security, and smart cities.
Milesight’s 5G AIoT Network Camera Demonstrated…
READ NOWThis year’s LoRaWAN® World Expo, held in Paris in early July, featured a wealth of information exchanged by leading industry figures from around the world. The live event was a true success with more than 1,200 attendees from 68 countries – the largest LoRa Alliance® event ever held.
The LoRaWAN® World Expo: The Power of LoRaWAN
READ NOWThe Need for Continuous Asset Tracking
Of the many complexities along the global supply chain and daily logistics operations, asset tracking is arguably the most challenging. Disruptions and subsequent capital loss not only affect goods transported worldwide, but also containers and vehicles used for shipment. On a more local scale, retail stores and shop owners are challenged in keeping track of their assets and supply at all times throughout the day for reasons varying from theft prevention to inventory management.
LoRa Cloud Locator Service Evaluates Asset…
READ NOWThe increasing demand for intelligent, scalable and cost-effective global asset tracking solutions is a trend, which has been recently accelerated by the urgency to improve end-to-end supply chain performance, visibility and customer services.
Semtech Expands LoRa Edge With Multi-Band LoRa…
READ NOWLogin to mySemtech to access product documentation for assistance with prototyping and production.
Find support and additional resources specifically for LoRa at the links below.