The SparkFun MAX-M10S Breakout is an ultra-low-power, high performance, miniaturized GNSS board that is perfect for battery operated applications that don't possess a lot of space, such as asset trackers and wearable devices. The MAX-M10S module from u-blox has an extremely low power consumption that is less than 25mW in continuous tracking mode.
The on-board MAX-M10S GNSS receiver can receive signals from the GPS, GLONASS, BeiDou, and Galileo constellations. Thanks to the u-blox Super-S technology, the module offers improved RF sensitivity with small antennas and in non-line-of-sight scenarios. We've included an SMA connector for a sturdy connection when attaching an external antenna. The board is also equipped with an on-board rechargeable battery that provides backup power to the module's RTC. This reduces the time-to-first fix from a cold start (~24s) to a hot start (~1s). The battery will maintain RTC and GNSS orbit data without being connected to power for up to five hours. This increases precision and decreases lock time in battery operated devices without compromising GNSS performance.
Additionally, this u-blox receiver supports I2C which makes it perfect for Qwiic compatibility so we don't have to use up our precious UART ports. Utilizing our handy Qwiic system, no soldering is required to connect it to the rest of your system. However, we still broke out 0.1"-spaced pins in case you prefer to use a breadboard. For users that prefer to communicate over UART, we made sure to configure the UART pin grouping to an industry standard to ensure that it easily connects to a Serial Basic.
U-blox based GNSS products are configurable using the popular Windows program called u-center. Plenty of different functions can be configured on the MAX-M10S: baud rates, update rates, spoofing detection, external interrupts, etc. We've also written an extensive Arduino library for u-blox modules to make reading and controlling the MAX-M10S over our Qwiic Connect System easy. Leave NMEA behind! Start using a much lighter weight binary interface and give your microcontroller (and its one serial port) a break. The SparkFun Arduino library shows how to read latitude, longitude, even heading and speed over I2C without the need for constant serial polling.
Note: The I2C address of the MAX-M10S is 0x42 and is software configurable. A multiplexer/Mux is required to communicate to multiple MAX-M10S boards with the same address on a single bus. If you need to use more than one MAX-M10S with the same address consider using the Qwiic Mux Breakout.
The SparkFun Qwiic Connect System is an ecosystem of I2C sensors, actuators, shields and cables that make prototyping faster and less prone to error. All Qwiic-enabled boards use a common 1mm pitch, 4-pin JST connector. This reduces the amount of required PCB space, and polarized connections mean you can’t hook it up wrong.
We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.
Based on 5 ratings:
1 of 1 found this helpful:
very good.
1 of 1 found this helpful:
Works great. I built an open-source ESP32 NTP Time Server with it, to find it just search for 'esp32 time server stratum 1' on hackaday.
Also, I had a support question regarding its Sparkfun library, and that question was answered very quickly and professionally.
Well done Sparkfun!
0 of 1 found this helpful:
This board only works with UART on the Raspberry Pi, and that requires soldering the serial pins which I wanted to avoid and is why I bought the qwiic board. It's a bug in the RasPi i2c implementation, not this board, but that doesn't help me. I really wish this had been documented in the product page as I would have bought something else.
This is a solid product and easy to get up and running. I am running it as a serial device on a Nvidia Jetson Nano development board as part of a telescope automation project.
It works as expected. Being used in a chain of other sensors with the Open Log Artemis.
hey
From what I understand this GNSS module only works with active antennas right? Passive antennas like the ones sparkfun sell don't work? https://www.sparkfun.com/products/15247
best regards
I've used the MAX-M10S with passive (chip) antennas. It works, but it's generally a frustrating experience as the gain on chip antennas is low so you will need a very clear sky with lots of time to achieve lock (think 5 to 10 minutes rather than 30 to 60 seconds).